AXIS#.VL.FBSOURCE
Description
This parameter determines the feedback source to be used by the velocity loop.
Value | Definition |
---|---|
0 | Defers selection to AXIS#.IL.FBSOURCE - this is the default, and uses the value which is being used for commutation |
1 | Selects FB1 (connector X1) |
2 | Selects FB2 (connector X2) |
3 | Selects FB3 (connector X23) |
4 | Selects FB4 (connector X21) |
5 | Selects FB5 (connector X22) |
-
- If Axis 2 has been configured to use gantry command source (AXIS#.CMDSOURCE = 4) and the gantry is active (GANTRY.STATE = 3), if this keyword is changed, it will set the gantry state back to "pending homing" (GANTRY.STATE = 1). See GANTRY.HOME.REQUIRED documentation for more details.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 5 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics